Edmund Optics® は当社ウェブサイトの技術サービス機能最適化のため、自社並びに第三者のクッキーを使用します。当社クッキーの取り扱いについて

  • マイアカウント
  •   
Resources / アプリケーションノート / レーザー / Importance of Beam Diameter on Laser Damage Threshold
Importance of Beam Diameter on Laser Damage Threshold

Importance of Beam Diameter on Laser Damage Threshold

This is Section 3.5 of the Laser Optics Resource Guide.

The diameter of a laser highly affects an optic’s laser induced damage threshold (LIDT) as beam diameter directly influences the probability of laser induced damage.1 When the beam size of a laser used for LIDT testing is significantly larger than the density of defects on the optic, the likelihood of triggering scarce damage mechanisms is high - these unlikely events are detectable. If the beam size is too small, low defect densities are not always detectable and parts appear more resistant to damage than they actually are (Figure 1).

Figure 1: Small diameter beams are less likely to overlap with low density defects on an optic undergoing testing, resulting in overly optimistic LIDT values
Figure 1: Small diameter beams are less likely to overlap with low density defects on an optic undergoing testing, resulting in overly optimistic LIDT values

The smallest beam diameter permitted for LIDT testing in ISO 21254 is 0.2mm. Many laser optics suppliers prefer to use as small of a beam as possible because it is easier to achieve a high fluence, although this may lead to an “under-sampling” of the surface. Figure 2 demonstrates how laser damage scales with the diameter of a beam. In the scenario shown, a large number of the defects have a threshold fluence of 10J and a small number have a threshold fluence of 1J. This simplified model provides insight for real world usage, as laser optics typically contain various types of defects with different densities and individual damage thresholds. Scaling the beam diameter from 0.2mm to 10mm will drastically change the damage probability function and therefore change the LIDT value concluded from the test. With a 0.2mm beam, the chance of detecting one of the 1J threshold defects is small. For this reason, the damage probability will remain very low until a fluence of 10J is reached. Increasing the beam size from 0.2mm to 2mm makes detecting 1J threshold defects more likely, thereby causing a sharp increase in damage probability at a fluence of 1J. When the beam diameter is scaled to 10mm, the damage probability at 1J increases to an almost certain probability of damage.

Figure 2: In this example with 2 different defect types, LIDT drops by a factor of 10 when scaling the beam size from 0.2mm to 10mm
Figure 2: In this example with 2 different defect types, LIDT drops by a factor of 10 when scaling the beam size from 0.2mm to 10mm

While LIDT scales with changes in wavelength and pulse duration, it also scales with beam diameter. For small changes in beam diameter, this scaling can be approximated by multiplying the original LIDT value by the square of the ratio of the original diameter to the new diameter.1

(1)$$ \text{LIDT} \! \left( \lambda_2 , \tau_2 , ∅_{2} \right) = \text{LIDT} \! \left( \lambda_1 , \tau_1 , ∅_{1} \right) \times \left( \frac{\lambda_2}{\lambda_1} \right) \times \sqrt{\frac{\tau_2}{\tau_1}} \times \left( \frac{∅_1}{∅_2} \right) ^2 $$


Reference

  1. L. Gallais, J. Capoulade, J.-Y. Natoli and M. Commandré, "Investigation of nanodefect properties in optical coatings by coupling measured and simulated laser damage statistics," J. Appl. Phys, vol. 104, p. 053120, 2008.
このコンテンツはお役に立ちましたか?

With this application note, learn all about lasers including the elements, mounting, how they work, and the accessories.

 レーザー損傷閾値 (LDT) について理解し、あなたのレーザーオプティクスへの損傷を回避して、優れた成果と製品寿命の長期化を実現しましょう。

These EO application notes will help you prepare for your next laser setup.

エドモンド・オプティクスは、正しいイメージングレンズの特定方法をサポートするだけでなく、あなたのイメージングに対するニーズを上回る様々な資料や製品を用意することができます。

お見積りは必要ですか?

Edmund Optics Facebook Edmund Optics Twitter Edmund Optics YouTube Edmund Optics LinkedIn Edmund Optics Instagram

×