Edmund Optics® は当社ウェブサイトの技術サービス機能最適化のため、自社並びに第三者のクッキーを使用します。当社クッキーの取り扱いについて

  • マイアカウント
  •   
Resources / 専門用語 / N

Glossary: N

NIR (Near Infrared)

The portion of the electromagnetic spectrum from 700 to 1100nm. Definition may differ by application.

Neutral Density Filter (ND)

A type of filter that yields a constant attenuation, or optical density, value over a range of wavelengths (i.e. spectrally flat). It is useful for attenuating, or reducing, the amount of light in a system.

Noise

Caused by the unwanted spontaneous emission of light from a laser medium resulting in reduced optical performance.

Noise Equivalent Power (NEP)

The incident light power required to produce a signal on a detector that is equal to the noise. In this case, the signal-to-noise ratio is equal to one.

Non-Polarizing Beamsplitter

A type of beamsplitter that splits the incident light by a specific percentage without altering the polarization state of the transmitted or reflected light.

  See also Polarization , Beamsplitter

Normal Load Capacity

The maximum downward (compression) load or force that can be applied to a mechanical component perpendicular to the mounting surface. The center of force, or the center of gravity, of the load must be located in the center of the mounting surface.

Notch Filter

A type of filter designed to block a pre-selected bandwidth while transmitting all other wavelengths within the design range of the filter.  Manufactured using the dielectric stack method which involves using a series of thin layers of dielectric materials, of alternating refractive index.

Nth Order

Multiple combinations of wavelength and integer order values that will satisfy any given groove spacing, angle of incidence, and diffracted angle calculated from the grating equation. Gratings are generally specified in terms of first order diffraction since efficiency decreases with higher orders.

Numerical Aperture (NA)

The sine of the vertex angle of the largest cone of meridional rays that can enter or exit an optical system. In other words, it governs the amount of light entering or exiting a system. It is inversely related to the f/#.

Nyquist Limit

The theoretical limit of a camera's resolution or sampling ability, defined as the inverse of twice the pixel size. 

  See also Pixel

当社の専門性は、球面素子、非球面レンズ、プリズム、イメージングレンズ、イメージングやレーザー用オプティクスの組立品、メカニクスだけに留まりません。

エドモンド・オプティクスには、可能な中でのベストソリューションを提供できるエンジニアの専門家がいます。在庫販売製品から特注デザインまで、EOはあなたのニーズに適合させるのに必要な業界と技術的知識があります。

アメリカ、ヨーロッパ、アジアの各地に15以上の現地オフィスを配置。世界水準のサービスで現地サポートをご提供しています。

エドモンド・オプティクスでは、お客様のニーズに合わせてさまざまなサービスをご用意しています。是非ご活用ください。

お見積りは必要ですか?

Edmund Optics Facebook Edmund Optics Twitter Edmund Optics YouTube Edmund Optics LinkedIn Edmund Optics Instagram

×