Effective Focal Length, EFL (mm): --
Back Focal Length, BFL (mm): --
Front Focal Length, FFL (mm): --
Primary Principal Point, P (mm): --
Secondary Principal Point, P'' (mm): --
Shift in Nodal Point (mm): >--
ΦOS | Power of Surface 1 |
ΦIS | Power of Surface 2 |
F | Lens Power |
nOS | Object Space Index |
nL | Lens Index |
nIS | Image Space Index |
R1 | Radius of Surface 1 |
R2 | Radius of Surface 2 |
CT | Center Thickness |
P | Primary Principle Point |
P" | Secondary Principle Point |
EFL | Effective Focal Length |
BFL | Back Focal Length |
FFL | Front Focal Length |
NPS | Nodal Point Shift |
fF | Front Focal Point |
fR | Rear Focal Point |
Note: This calculator follows the standard sign convention for the optical radius of curvature where if the vertex of a surface lies to the left of the center of curvature the radius of curvature is positive, and if the vertex lies to the right of the center of curvature the radius of curvature is negative. In the figure, R1 is positive and R2 is negative.
Relate optical and mechanical parameters of simple lenses in order to ease integration into application assemblies. Select index from list of EO's own optical substrates to help calculate focal lengths and principal points of any standard lens.