Edmund Optics® は当社ウェブサイトの技術サービス機能最適化のため、自社並びに第三者のクッキーを使用します。当社クッキーの取り扱いについて

  • マイアカウント
  •   
Resources / 専門用語 / V

Glossary

Varifocal

Low magnification lens which has a variable focal length, but which requires refocus with adjustment.

Vernier

For rotary stages, a scale measuring the amount of angular movement by the drive. Vernier values of resolution are the smallest angular movement that can be measured by the scale.

Vibration Rating

Measure of the vibrational durability of a component within a certain range of frequencies, expressed in units of acceleration (G).

Viewing Angle

For light control film, the full angle through which the film will transmit light. This value is centered about the louver angle of the film.

  See also Louver Angle

Vignetting

A fall-off in illumination of the image.  This can occur when the sensor is larger than the specified maximum sensor size of the lens is used or can naturally occur due to limitations of the geometry of the system.

VIS Coating

BBAR coating optimized for use in the visible spectrum between 425 nm and 675nm. Does not transmit NIR efficiently.

VIS/NIR Coating

BBAR coating optimized for use from 425nm to 900nm with good transmission out to 1000nm.

Viscosity

A measure of a fluid's resistance to flow, or the ratio of shearing stress to the velocity gradient.  Water is a low viscosity fluid while peanut butter has a high viscosity.  

Visible Spectrum

The part of the electromagnetic spectrum from approximately 400 - 750nm. 

当社の専門性は、球面素子、非球面レンズ、プリズム、イメージングレンズ、イメージングやレーザー用オプティクスの組立品、メカニクスだけに留まりません。

エドモンド・オプティクスには、可能な中でのベストソリューションを提供できるエンジニアの専門家がいます。在庫販売製品から特注デザインまで、EOはあなたのニーズに適合させるのに必要な業界と技術的知識があります。

アメリカ、ヨーロッパ、アジアの各地に15以上の現地オフィスを配置。世界水準のサービスで現地サポートをご提供しています。

エドモンド・オプティクスでは、お客様のニーズに合わせてさまざまなサービスをご用意しています。是非ご活用ください。

お見積りは必要ですか?

Edmund Optics Facebook Edmund Optics Twitter Edmund Optics YouTube Edmund Optics LinkedIn Edmund Optics Google+ Edmund Optics Instagram

×