Edmund Optics®, a leading global provider of optical and imaging technology solutions, has expanded its portfolio of motorized stages, bringing together in-stock availability with a broad range of configurable motion solutions for industrial or scientific applications.
The offering supports both fully motorized, software-controlled systems as well as modular mechanical stages with added motorization. This allows users to select an approach that best fits their application whether they require a full, plug-and-play motorized system or a more flexible configuration built around mechanical setups.
The wide selection of off-the-shelf motorized stages and accessories enables fast procurement and flexible system build. For multi-axis applications, software-driven stage families, like those from Zaber™, streamline integration and control through features such as native daisy-chain connectivity and virtual configuration tools, enabling users to validate system setups in advance.
For applications requiring high mechanical stability and precision, Edmund Optics offers TECHSPEC® motorized stage designs with rigid, monobloc construction that reduce alignment errors and improve positioning accuracy. These systems support a high level of compatibility across TECHSPEC® components, enabling combinations of motorized and manual axes within the same setup, as well as options for piezo-assisted motion when fine positioning is required.
The range includes a variety of motorized stage configurations, from linear to rotary motion, designed to support a wide range of applications. Additional options are available for vacuum and life science environments, along with a selection of compatible accessories. By combining a broad selection of in-stock motorized systems with complementary mechanical solutions in a single portfolio, Edmund Optics enables customers to efficiently source motion systems while maintaining the flexibility to adapt designs as requirements evolve. This is further supported by a catalogue of over 34,000 optics, imaging, and photonics components, offering a convenient, single-source solution for complete motion and optical system integration.
About Edmund Optics:
With over 80 years of experience, Edmund Optics® is a trusted provider of high-quality optical components and solutions, serving industries like Life Sciences, Biomedical, Industrial Inspection, Semiconductor, and R&D. The company employs 1,300+ people across 19 global locations and continues to grow.
As a leading optics and photonics company, Edmund Optics provides two specialized solutions: a robust Marketplace with 34,000+ off-the-shelf products and Advanced Manufacturing, which focuses on custom and volume production of precision optical and imaging components.
Edmund Optics’ Marketplace is a one-stop shop for over 34,000 in-stock products from in-house manufacturing and 40+ top-tier brands, covering the entire beam path with fast, easy purchasing. For tailored solutions, Advanced Manufacturing offers custom design, first-article production, and scalable manufacturing — supported by four global design centres and nine specialized factories producing over 2 million components and 175,000+ assemblies annually.
Learn more at www.edmundoptics.com.
Contact:
Agnes Huebscher
Senior Director Corporate Affairs, Communications and Industry Relations
ahuebscher@edmundoptics.de
もしくは 現地オフィス一覧をご覧ください
クイック見積りツール
商品コードを入力して開始しましょう
Copyright 2023, エドモンド・オプティクス・ジャパン株式会社
[東京オフィス] 〒113-0021 東京都文京区本駒込2-29-24 パシフィックスクエア千石 4F
[秋田工場] 〒012-0801 秋田県湯沢市岩崎字壇ノ上3番地
The FUTURE Depends On Optics®